Download document () of 20

Soft starter or VFD?

How to choose between a soft starter and a variable frequency drive

Motors often require large amounts of energy when quickly accelerating to full speed. Soft starters and variable frequency drives can both be used to reduce inrush currents and limit torque – protecting your valuable equipment and extending the life of your motor by reducing motor heating caused by frequent starts and stops.

Choosing between a soft starter and a variable frequency drive often depends on the application, system requirements and cost (both for initial start-up and over the life cycle of the system). 

Variable frequency drive product

Variable frequency drives

A variable frequency drive (VFD) is a motor control device that protects and controls the speed of an AC induction motor.

A VFD can control the speed of the motor during the start and stop cycle as well as throughout the run cycle.

VFDs are also referred to as adjustable frequency drives (AFDs).

Soft starter product

Soft starters

A soft starter is a solid-state device that protects AC electric motors from damage caused by sudden influxes of power by limiting the large initial inrush of current associated with motor start-up.

They provide a gentle ramp up to full speed and are used only at start-up (and stop, if equipped). Ramping up the initial voltage to the motor produces this gradual start.

Soft starters are also known as reduced voltage soft starters (RVSS).

Applications

Variable frequency drive applications

VFDs are used in applications where:

  • Complete speed control is required
  • Energy savings is a goal
  • Customised control is needed

Soft starter applications

Soft starters are used in applications where:

  • Speed and torque control are required only during start-up (and stop if equipped with soft stop)
  • Reducing large start-up inrush currents associated with a large motor is required
  • The mechanical system requires a gentle start to relieve torque spikes and tension associated with normal start-up (for example, conveyors, belt-driven systems, gears and so on)
  • Pumps are used to eliminate pressure surges caused in piping systems when fluid changes direction rapidly

How they work

How do VFDs work?

VFDs convert input power to adjustable frequency and voltage source for controlling speed of AC induction motors. The frequency of the power applied to an AC motor determines the motor speed, based on the following equation:

N = 120 x f x p

N = speed (rpm)
f = frequency (Hz)
p = number of motor poles

For example, a four-pole motor is operating at 60 Hz. These values can be inserted into the formula to calculate the speed:

N = 120 x 60 x 4
N = 1800 (rpm)

  • AC supply: Comes from the facility power network (typically 480 V, 60 Hz AC)
  • Rectifier: Converts network AC power to DC power
  • Filter and DC bus: Work together to smooth the rectified DC power and to provide clean, low-ripple DC power to the inverter
  • Inverter: Uses DC power from the DC bus and filter to invert an output that resembles sine wave AC power, using a pulse width modulation (PWM) technique
  • Pulse width modulation: Switches the inverter semiconductors in varying widths and times that, when averaged, create a sine waveform

How does a soft starter work?

Electrical soft starters temporarily reduce voltage or current input by reducing torque. Some soft starters may use solid-state devices to help control the flow of the current. They can control one to three phases, with three-phase control usually producing better results.

Most soft starters use a series of thyristors or silicon controlled rectifiers (SCRs) to reduce the voltage. In the normal OFF state, the SCRs restrict current, but in the normal ON state, the SCRs allow current. The SCRs are engaged during ramp-up and bypass contactors are pulled in after the maximum speed is achieved. This helps to significantly reduce motor heating.

Robotic tank welding system on conveyor belt

Benefits of each

Benefits of choosing a VFD

  • Energy savings
  • Reduces peak energy demand
  • Reduces power when not required
  • Fully adjustable speed (pumps, conveyors and fans)
  • Controlled starting, stopping and acceleration
  • Dynamic torque control
  • Provides smooth motion for applications such as lifts and escalators 
  • Maintains speed of equipment, making drives ideal for manufacturing equipment and industrial equipment such as mixers, grinders and crushers
  • Versatility
  • Self-diagnostics and communication
  • Advanced overload protection
  • PLC-like functionality and software programming
  • Digital inputs/outputs (DI/DO)
  • Analogue inputs/outputs (AI/AO)
  • Relay outputs

Energy savings

VFDs offer the greatest energy savings for fans and pumps. The adjustable flow method changes the flow curve and drastically reduces power requirements.

Centrifugal equipment (fans, pumps and compressors) follow a general set of speed affinity laws. The affinity laws define the relationship between speed and a set of variables:

  • Flow
  • Pressure
  • Power

Based on the affinity laws, flow changes linearly with speed while pressure is proportional to the square of speed. The power required is proportional to the cube of the speed. The latter is most important, because if the motor speed drops, the power drops by the cube.

Benefits of choosing a soft starter

Soft starters are often the more economical choice for applications that require speed and torque control only during motor start-up. Additionally, they are often the ideal solution for applications where space is a concern, as they usually take up less space than variable frequency drives.

oil-rig-LED-lights.jpg

Selecting the correct equipment for your needs

Choosing a soft starter or a variable frequency drive often depends on your application. Soft starters are smaller and less expensive when compared with VFDs in larger horsepower applications. Larger VFDs take up more space and are usually more expensive than soft starters.

That being said, while a VFD is often more expensive up front, it can provide energy savings of up to 50%, thereby producing more cost savings over the life of the equipment.

Speed control is another advantage of a VFD, because it offers consistent acceleration time throughout the entire operating cycle of the motor, not just during start-up. VFDs can also provide more robust functionality than soft starters offer, including digital diagnostic information.

It is important to note that a VFD can initially cost two to three times more than a soft starter. Therefore, if constant acceleration and torque control is not necessary and your application requires current limiting only during start-up, a soft starter may be a better solution from a cost standpoint.