Download document () of 20

Fundamentals of automatic transfer switches (ATS)

What is an automatic transfer switch?

Low-voltage automatic transfer switch assemblies provide a reliable means of transferring essential load connections between primary and alternate sources of electrical power. Data centres, hospitals, factories and a wide range of other facility types that require continuous or near-continuous uptime typically use an emergency (alternative) power source such as a generator or a back-up utility feed when their normal (primary) power source becomes unavailable. 
eaton-transfer-switch-family-image-2019.jpg

A typical transfer sequence includes:

  1. The normal utility power source fails.
  2. The transfer switch shifts the load to the emergency power source when power from the generator or back-up utility feed is stable and within prescribed voltage and frequency tolerances. Depending on the facility’s needs and preferences, the transfer process is self-acting or manually-initiated.
  3. The transfer switch returns the load from the emergency power source to the normal power source when utility power is restored. The retransfer process is self-acting or manually-initiated.

What ATS arrangements are available?

A variety of arrangements are available, using two and three power sources.

Two power sources

Utility – generator

The standard transfer switch configuration includes an electric utility service and a generator for normal and emergency power sources. This system arrangement is typically referred to as an emergency standby generator system. The single generator shown may be several engine-generator sets operating in parallel.

automatic-transfer-swtich-drawing-util-gen.jpg

Utility – utility

This use case employs two utility sources that provide redundancy in the distribution system and allows for quick restoration of service to the load if an upstream equipment failure occurs. The two sources can be independent of each other, requiring the public utility company to provide dual electric services, or they can originate from a single electric service that is distributed through redundant paths within the facility. 

automatic-transfer-swtich-drawing-util-util.jpg

Generator – generator

Transfer switches, at times, are applied between two generator sets for prime power use, often at remote installations. In such cases, the generator may be required to provide continuous power 24/7.  To equally share run-time, source power is periodically alternated between the generator sets.

automatic-transfer-swtich-drawing-gen-gen.jpg

Three power sources

Utility – generator – generator

Critical facilities with an emergency standby generator system will often include provisions for a second generator connection to serve as a redundant emergency back-up that can be used during periods of inclement weather or when scheduled maintenance is being performed on the first generator.

As shown, in some cases, the first generator is permanently installed onsite whereas the second generator will be a portable roll-up type that is deployed when needed. 

automatic-transfer-swtich-drawing-util-gen-gen-example22.jpg
automatic-transfer-swtich-drawing-util-gen-gen-example -1.jpg

Utility – utility – generator

This configuration expands on the redundancy provided by a dual utility arrangement and includes an emergency standby generator source.  As shown, the generator can be dedicated for use by a single transfer switch or shared among multiple transfer switches employing a priority control scheme.  

automatic-transfer-swtich-drawing-util-util-gen-example-2.jpg
automatic-transfer-swtich-drawing-util-util-gen example-1.jpg

Different ATS transition types

Transfer switches transition loads between normal and emergency power sources with open or closed options. The specific functions performed by a given load and the importance of those functions to safety or security play an important role in determining which kind of transition is required.

 

Open transition

An open transition is a break-before-make transfer. The transfer switch breaks its connection to one power source before making a connection to the other. Open transitions include open-delayed and open in-phase.

 

Closed transition

A closed transition is a make-before-break transfer. The transfer switch makes a connection to a second power source before breaking its connection with the first power source. As there’s no gap between disconnection and connection, downstream loads receive continuous power throughout the transfer process. 

ATS open transition 1300x800
ATS closed transition 1300x400

ATS modes of operation

Manual

Transfer initiation and operation are performed manually, typically by pushing a button or moving a handle; initiation occurs locally

Non-automatic

Manually initiate a transfer by pressing a button or rotating a switch to cause an internal electromechanical device to electrically operate the switching mechanism; initiation can occur locally or remotely

Automatic

Transfer switch controller is self-acting and completely manages both initiation and operation; initiation is triggered when the automatic controller senses an unavailability or loss of source power followed by operation of the switching mechanism

What types of switching mechanisms are available? 

The switching mechanism is the part of a transfer switch that is physically responsible for carrying the rated electrical current and shifting the load connection from one power source to another. These include: 

Contactor type

This is the most common and typically most economical switching mechanism type. Contactors are constructed as an electrically-controlled, double-throw switch where a single operator opens one set of power contacts while closing a second set.

contactor-switching-mechanisms.png

Moulded case type

Routinely used for closing and interrupting a circuit between separable contacts under both normal and abnormal conditions, moulded case switches feature simple designs and are capable of supporting either a mechanically operated, over-centre toggle or a motor operator.

pd-circuit-breaker-molded-case-500x500.jpg

Power frame type

Power frame switches are larger, faster and more powerful than moulded case switches and are capable of handling up to 5,000 amps.  A two-step stored energy technology is used that permits manual and electrical operation under load.  

eaton-magnum-family-product-group.png

How do ATSs vary by application?

Switched neutral

For three-phase power applications requiring that the neutral conductor be switched, transfer switches can be configured with a fully-rated fourth pole that performs identically to the individual phase (A, B, C) power poles. For single-phase applications, a fully-rated third pole can be configured. A switched neutral is commonly used when the transfer switch is fed by separately derived power sources.

 

Bypass isolation automatic transfer switches

For simplified maintenance and improved uptime, bypass isolation automatic transfer switches provide dual switching functionality and redundancy for critical applications. The primary ATS handles the day-to-day distribution of electrical power to the load, while the bypass switch serves as a back-up or redundant device.

A bypass isolation transfer switch is frequently selected for use in healthcare and other critical applications because it allows the ATS – and in some cases the bypass switch – to be drawn out and isolated from the power source(s) to facilitate regular maintenance, inspection and testing as prescribed by code (NFPA 110).

 

Service entrance transfer switches

Facilities with a single utility connection and a single emergency power source will often have an ATS located at the service entrance to ensure that critical loads can quickly and safely shift to emergency power if utility power is interrupted. Non-critical loads are often inhibited or shed from connection to the emergency power source to avoid capacity overload.

 

Ratings

When applying a transfer switch for use in a power distribution system, consideration must be given to the closing current tolerance rating to ensure system integrity and reliability. The UL1008 standard permits transfer switches to be marked with one or more short-circuit and/or short-time current tolerance rating specific to an overcurrent protection device type. Transfer switches with multiple ratings provide greater application flexibility.

Bypass-Isolation-Contactor-Type-ATS.jpg

Interested in finding out more?