Download document () of 20
We make what matters work*
Services

Synchronous condensers design and conversion

Amid today’s changing landscape of generation sources and regulatory requirements, Eaton’s synchronous condensers provide turnkey solutions to help utility companies enhance grid stability, reliability and dynamic reactive power compensation. Enabling utilization of existing assets in the wake of coal power plant retirements, each synchronous condensers project is customized to a utility’s specific needs.

Core features

  • Supports voltage during peak conditions and system disturbances with the ability to produce or consume reactive power
  • Provides fault current capacity to the system 
  • Dynamic voltage control supports high-level adaptive voltage control strategies
  • Inertia provided to transmission system 
  • Reactive power compensation can be utilized alone or with other devices to regulate and control reactive power flows 
  • Addresses short-term overload with ability to supply many times rated output for short-time durations

Decades of expertise

With a long history of overseeing successful turnkey design/build projects including synchronous condensers conversion and new build projects, Eaton’s Electrical Engineering Services & Systems team is your single-source provider for designing, building and commissioning power system solutions.

A longstanding solution to address a new problem

As one of the oldest power system support technologies, synchronous condensers have made a resurgence in recent years as more modern power electronics designed to replace them are falling short in their capabilities. By providing core benefits such as reactive power compensation, dynamic voltage control and short-circuit capacity/overload capabilities, Eaton’s synchronous condensers help utilities achieve grid reliability, stability, inertia and strength.

Eaton's engineering services team

Eaton’s engineering services team is dedicated to understanding your business so we can optimize your power system for safety, reliability and efficiency. As one of the largest and most experienced teams in the industry, we offer a comprehensive portfolio of services and solutions tailored for every stage of a power system’s life cycle. Eaton strives to create a zero-incident culture through the implementation of our safety policy including division safety managers and layered risk assessments. Our team has experience with electrical power distribution equipment from all leading manufacturers and stands ready to support you, 24/7, wherever and whenever you need us.
Specifications
With a long history of overseeing successful turnkey design/build projects including synchronous condensers conversion and new build projects,  Eaton has the knowledge and expertise to be your single source provider — regardless of the application. The following is just a sampling of the array of successful deployments completed by our engineering services team.
case-study-sync-facility-1500x1500.jpg

New synchronous condensers facility design and commission

Problem: A power company needed to control system voltage at the delivery point of a 63 MW wind farm. 

Solution: One Eaton synchronous condensers was used to provide voltage stability and fault current capacity during peak load conditions and transmission events, with Eaton's engineering services team building around a TEWAC +27.5/–14 Mvar synchronous machine. 

Results: The system relies on a variable speed drive and 1000 hp pony motor to provide trouble-free starting and synchronization, while the control system operates the condenser to control the bus voltage at the 115V substation. Integrating switched capacitor banks into the scheme, the control system continuously biases the machine output to operate in an under-excited state, allowing for full dynamic response to system faults and contingency events. 

case-study-sync-facility-outside-1500x1500.jpg

Retiring coal-fired generation facility

Problem: The reactive capabilities of the transmission system would be adversely impacted by the utility’s decision to retire the generating assets. 

Solution: Eaton engineers converted three 165 MW steam turbine generators to synchronous condensers by disconnecting the turbine, replacing the excitation and control systems, and performing modifications to auxiliary systems. A PLC-based control system was implemented to handle machine startup, synchronizing and dispatch functions. 

Results: The control system ensures all machines work together to support the 138 kV bus voltage while sharing load equally among machines. 

 

case-study-sync-system-reliability-1500x1500.jpg

System reliability project

Problem: A utility company desired system reliability and voltage stability for overloaded transmission lines and frequent voltage excursions at its facility. 

Solution: Two water-cooled, 16 Mvar synchronous condensers using variable speed drives and 500 hp pony motors were implemented to support AC voltage during peak loading conditions and transmission system outages, as well as provide fault current capacity.  

Results: The Eaton synchronous condensers solution stabilized the system by supplying voltage control and short-circuit current strength, avoiding the need for more costly transmission system upgrades. 

 

Download Links
X
Download Close