Correctly sizing your UPS solution is the first step to developing an efficient system. The more closely the UPS capacity matches the load, the more efficiently the UPS will operate. However, a UPS with insufficient capacity may be unable to support your equipment during an outage or other power problem.
To find the proper balance, there are two major questions to consider: how much power is required to support connected equipment (capacity), and how long will the UPS need to support equipment during an outage (runtime)?
A UPS system's capacity rating is the maximum power that the unit can output to support connected equipment. It is typically measured in Volt Amps (VA). To ensure sufficient protection and account for growth, we recommend using a UPS that has a VA capacity rating that is greater than the total power needed for the protected equipment, by at least 15%.
Runtime refers to the amount of time that the UPS will be able to support connected equipment from battery for a given load level. Runtime is important because it tells you how long your equipment will continue to run during a power outage before the UPS battery runs out. You can increase runtime by selecting a UPS with a larger battery, or by adding external battery packs to a UPS that accepts them.
You'll need a UPS with enough capacity to handle the full load, as well as a battery system (either internal or with additional external battery packs) that can support that load for long enough to restore power or safely shut down your systems. Expected growth and redundancy requirements should also be considered. Eaton's UPS Finder is a tool that automates the sizing process, but we'll go through the calculation below:
Mission-critical loads demand an extra level of protection in case of human error or other failure. Sizing your UPS solution for redundancy can provide that extra level of protection. Redundancy can be achieved by connecting multiple UPS systems in parallel (or a modular UPS system) to a common critical load bus (e.g., an ATS PDU).
The most common redundancy architecture is N+1, where N refers to the number of units (or modules) required to support the load. Thus N+1 configurations include one more unit (+1) than the load requires. This means that if any one unit fails, the remainder can continue to support the critical load without interruption.
Sizing a solution based on 3-phase utility power can be tricky. Contact our 3-phase experts for sizing help.